:REPository:MEASure:PAM:LEVel:SELection:CLEar
Meas. mode:
Jitter
Waveforms:
PAM4
Publish mode:
Selected
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:MEASure:PAM:LEVel:SELection:CLEar
Description
For the Selected publishing mode, excludes all Jitter Mode PAM4 level measurements in the Level panel from being published. Use the :REPository:MEASure:PAM:LEVel:SELection:ALL
sibling command to include all PAM-level Results panel measurements. Use the :REPository:MEASure:PAM:LEVel:SELection
parent command to select specific PAM4 level Results panel measurements or the query form to return the currently selected measurements.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.