:REPository:MEASure:MTESt:SELection:ALL
Meas. mode:
Eye
Waveforms:
NRZ
Publish mode:
Selected
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:MEASure:MTEStN:SELection:ALL
Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2:
selects mask 2.
Description
For the Selected publishing mode, selects to publish all Eye Mode Mask Test measurements in the Mask Test panel. Use the :REPository:MEASure:MTESt:SELection:CLEar
sibling command to exclude all Mask Test panel measurements. Use the :REPository:MEASure:MTESt:SELection
parent command to select specific Mask Test panel measurements or the query form to return the currently selected measurements.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.