:REPository:MEASure:EYE:SELection:CLEar
Meas. mode:
Eye
Waveforms:
NRZ
PAM4
Publish mode:
Selected
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:MEASure:EYE:SELection:CLEar
Description
For the Selected publishing mode, prevents all Eye Mode measurements in the Results panel from being published. Use the :REPository:MEASure:EYE:SELection:ALL
sibling command to include all Results panel measurements. Use the :REPository:MEASure:EYE:SELection
parent command to select specific Results panel measurements or the query form to return the currently selected measurements.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.