:SLOT:TRIGger:TRACking
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SLOTN:TRIGger:TRACking {ON | OFF | 1 | 0}
Where N identifies a specific module by slot and must be selected from {1:8}.
Query Syntax
:SLOTN:TRIGger:TRACking?
Query Response
{1 | 0}
Description
When using pattern lock, turns on pattern lock tracking where pattern lock settings are the same (linked) for all DCA-M and 86100D oscilloscopes. The clock and data signals should be the same rate and pattern length. The default setting is on.
This command applies to an N1092A/B/D Option-PLK DCA-M.