:SLOT:TRIGger:DCDRatio

Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:SLOT{1:8}:TRIGger:DCDRatio  {UNITy | SUB2 | SUB4 | …}

Where the {1:8} specifier identifies a module slot.

Query Syntax

:SLOT{1:8}:TRIGger:DCDRatio?

Description

When using pattern lock, enters the trigger-divide ratio. To apply the ratio, disable autodetection (:SLOT{1:8}:TRIGger:DCDRatio:AUTodetect). In some situations, you may need to enter a trigger divide ratio for a trigger that is a divided rate from the data rate. For example, for rates greater then 23.2 Gbs, you must provide a divided trigger.

DCDRatio Rate Arguments
Rate Argument
1:1 (Sub-Rate) UNITy
1:2 (Sub-Rate) SUB2
1:4 (Sub-Rate) SUB4
1:5 (Sub-Rate) SUB5
1:8 (Sub-Rate) SUB8
1:10 (Sub-Rate) SUB10
1:15 (Sub-Rate) SUB15
1:16 (Sub-Rate) SUB16
1:18 (Sub-Rate) SUB18
1:20 (Sub-Rate) SUB20
1:24 (Sub-Rate) SUB24
1:25 (Sub-Rate) SUB25
1:30 (Sub-Rate) SUB30
1:32 (Sub-Rate) SUB32
1:35 (Sub-Rate) SUB35
1:36 (Sub-Rate) SUB36
1:40 (Sub-Rate) SUB40
1:45 (Sub-Rate) SUB45
1:50 (Sub-Rate) SUB50
1:64 (Sub-Rate) SUB64
1:66 (Sub-Rate) SUB66
1:100 (Sub-Rate) SUB100
1:128 (Sub-Rate) SUB128

This command applies to an N1092A/B/D Option-PLK DCA-M.

Example Command Sequence

:SLOT2:TRIGger:DCDRatio:AUTodetect OFF 
:SLOT2:TRIGger:DCDRatio SUB2
:TRIGger:PLOCk