:SLOT:TRIGger:RSYmbol:SCTimebase
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SLOT{1:8}:TRIGger:RSYmbol:SCTimebase
Where the {1:8} specifier identifies a module slot.
Description
Realigns the timebase to use the left edge of the screen as the reference symbol for the pattern. For DCA-X oscilloscopes, use the :TRIGger:RSYMbol:SCTimebase command.
You can first position a symbol at the screen's left edge using one of the following two methods:
- Use the Find symbol sequence dialog. In FlexDCA's menu, click Tools > Find.... Or, use the
:TIMebase:Find:Sequenceand:TIMebase:FIND:NEXTcommands as show here:
:TIMebase:FIND:SEQuence "1101" :TIMebase:FIND:NEXT
:TIMebase:UNITs and :TIMebase:UIRPosition commands.:TIMebase:UNITs UINTerval :TIMebase:UIRPosition 8.8E+1
To automatically determine the reference symbol for the pattern and align the timebase with the reference symbol use the :SLOT:TRIGger:RSYMbol:AUTodetect command.
This feature is only available in Scope mode.
Requires FlexDCA revision A.06.71 and above.
Example Command
:SLOT2:TRIGger:RSYmbol:SCTimebase