:SLOT:TRIGger:PLENgth
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SLOT{1:8}:TRIGger:PLENgth <bits>
<bits> is an int.
Where the {1:8} specifier identifies a module slot.
Query Syntax
:SLOT{1:8}:TRIGger:PLENgth?
Description
When using pattern lock, enters the length of the test pattern in symbols. You must first disable automatic pattern-length detection (:SLOT{1:8}:TRIGger:PLENgth:AUTodetect OFF) before manually entering the pattern length. The command query returns the pattern length setting in symbols regardless of whether automatic detection is on or off.
To set or query the pattern length on simulated channels, use the :SOURce:PLENgth command.
This command applies to an N1092A/B/D Option-PLK DCA-M.
Example Command Sequence
:SLOT2:TRIGger:PLENgth:AUTodetect OFF :SLOT2:TRIGger:PLENgth 128