:SLOT:TRIGger:MRATe?
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:SLOT{1:8}:TRIGger:MRATe?
Where the {1:8} specifier identifies a module slot.
Description
Returns the measured clock rate at the Clock In input of a DCA-M oscilloscope. The query requires that the following be true:
- At least one of the DCA-M channel's needs to be on (although the channel input data does not need to be connected)
- There has been at least one data acquisition. (
:ACQuire:RUNor:ACQuire:SINGle)
Query Response
The query returns 9.91E+37 (NaN) if a DCA-M is not connected to the indicated slot.
| Response | Description |
|---|---|
| valid clock rate | A valid clock rate. For example, 9.95300E+9. |
0.000000000E+00
|
An attempt was made to acquire data, but there was no trigger signal (or very slow trigger) connected to the Clock In connector. |
-1.000000000E+00
|
The oscilloscope channel is off. Even if there is no signal connected to the channel, the channel must be turned on. |
9.91E+37
|
(NaN, Not A Number). A DCA-M oscilloscope is not connected to the indicated slot. |
This command applies to an N1090A or an N1092A/B/D DCA-M.
Compatible DCA-M Products
- N1094-series DCA-M sampling oscilloscopes
- N1092-series DCA-M sampling oscilloscopes
- N1090A DCA-M single optical channel sampling oscilloscope
Requires FlexDCA revision A.05.00 and above.
Example Command
:SLOT2:TRIGger:MRATe?