:SLOT:TRIGger:RSYMbol:AUTodetect
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SLOT{1:8}:TRIGger:RSYMbol:AUTodetect {ON | OFF | 1 | 0}
Where the {1:8} specifier identifies a module slot.
Query Syntax
:SLOT{1:8}:TRIGger:RSYMbol:AUTodetect?
Description
Automatically determines the reference symbol for the pattern and aligns the timebase with the reference symbol. The location is selected based on the longest run of symbols with a preference for lowest-level symbols. The pattern at the reference symbol is aligned to the display's left edge. To realign the timebase to use the left edge of the screen as the reference symbol for the pattern use the :SLOT:TRIGger:RSYmbol:SCTimebase command.
For DCA-X oscilloscopes, use the :TRIGger:RSYMbol:AUTodetect command.
Requires FlexDCA revision A.06.71 and above.
Example Command
:SLOT2:TRIGger:RSYMbol:AUTodetect ON