:SLOT:TRIGger:MODe?
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:SLOT{1:8}:TRIGger:MODe?
Where the {1:8} specifier identifies a module slot.
Description
Returns the trigger mode of a DCA-M product. The value returned is always CLOCk.
This command applies to an N1090A or an N1092A/B/D DCA-M.
Compatible DCA-M Products
- N1090A DCA-M single optical channel sampling oscilloscope
- N1092A/B/D DCA-M single optical channel sampling oscilloscope
Requires FlexDCA revision A.05.00 and above.
Example Command
:SLOT2:SLOT:TRIGger:MODe?