:SLOT:TRIGger:DCDRatio:AUTodetect
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SLOT{1:8}:TRIGger:DCDRatio:AUTodetect {ON | OFF | 1 | 0}
Where the {1:8} specifier identifies a module slot.
Query Syntax
:SLOT{1:8}:TRIGger:DCDRatio:AUTodetect?
Query Response
{1 | 0}
Description
Enables or disables automatic detection of trigger-divide-ratio for pattern lock. A default setup turns automatic detection on.
When automatic detection is turned off, use the :SLOT:TRIGger:DCDRatio command to enter the ratio. When automatic is enabled, send the :TRIGger:PLOCk ON or :SYSTem:PAUTodetect command to actually detect the trigger-divide-ratio.
This command requires that the type of Clock Ratio be first set to Integer instead of Fractional. Use the :SLOT:DCDRatio:TYPE command to select an integer clock ratio.
This command applies to an N1092A/B/D Option-PLK DCA-M.
Example Command Sequence
:SLOT2:DCDRatio:TYPE INTeger :SLOT2:TRIGger:DCDRatio:AUTodetect OFF :SLOT2:TRIGger:DCDRatio SUB4