:SYSTem:HELP:HEADers?

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL

Query Syntax

:SYSTem:HELP:HEADers?

Description

Returns a ASCII string of all FlexDCA programming commands and queries. Each line lists a command or query followed by a carriage return and line feed. If a command does not support a query, the line is ended with the "/nquery/" characters. If command only supports a query, the line is ended with the "/qonly/" characters. The first line of the returned data is the standard SCPI header for blocks of data. It specifies the data format and how much data will follow.

The following is an example of the first few lines returned by the query:

#6203607
:ACQuire:CDISplay/nquery/
:ACQuire:ECOunt
:ACQuire:ECOunt:DEFault
:ACQuire:ECOunt:MAXimum
:ACQuire:ECOunt:MINimum
:ACQuire:ECOunt:STEP/nquery/
:ACQuire:EPATtern
:ACQuire:EPATtern:DEFault
:ACQuire:EPATtern:TOGGle/nquery/
:ACQuire:EPATtern:VSET?/qonly/
:ACQuire:RLENgth
:ACQuire:RLENgth:AUTo
:ACQuire:RLENgth:AUTo:DEFault
:ACQuire:RLENgth:AUTo:NEXT/nquery/
………