:SYSTem:TEMPerature?
Instrument:
                                                N1010A
                                                N1000A
                                                DCA-M
                                            Meas. mode:
                                                Scope
                                                Eye
                                                Jitter
                                                TDR
                                            Flex Apps:
                                                FlexDCA
                                                FlexRT
                                            Query Syntax
:SYSTem:TEMPerature? [{FRAMe | SLOT{1:8} | CHAN{1:8}{A:D}}]
                                            Query Response
Returns a real. For example:
"-6.10"
Description
Returns a string of the temperature of the specified slot, channel, or N1000A mainframe. If no argument is specified, the temperature of the mainframe is returned. If the temperature of a simulated or empty slot or channel is queried, the value 9.91E+37 (NaN) is returned indicating the value is not a number.
Requires FlexDCA revision A.02.00 and above.
Example Commands
:SYSTem:TEMPerature? /* query the N1000A's temperature */ :SYSTem:TEMPerature? SLOT3 /* query temperature of module in slot 3 */