:SYSTem:OSYStem?
Instrument:
                                                N1010A
                                                N1000A
                                                DCA-M
                                            Meas. mode:
                                                Scope
                                                Eye
                                                Jitter
                                                TDR
                                            Flex Apps:
                                                FlexDCA
                                                FlexRT
                                            Query Syntax
:SYSTem:OSYStem?
Description
Returns a string that identifies the operating system under which the FlexDCA application is running. This is the same text that is shown in the About dialog (click Help > About), under the listing for OS. For example, when running embedded on an N1000A, a string that is similar to the following two strings could be returned:
- "Windows Embedded Standard 64 Bit"
 - "Microsoft Windows XP 32 Bit"
 
When running as an application on a PC, a string that is similar to the following is returned:
- "Windows 7 Enterprise 64 Bit"
 
Requires FlexDCA revision A.04.50 and above.