:SYSTem:SERial?
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:SYSTem:SERial? [{FRAMe | SLOT{1:8}}]
Description
Returns the serial number of FlexDCA or a module that is installed in the DCA-X.
- FRAMe
- Specifies the return of FlexDCA's serial number. This is the default argument if no argument is provided.
- SLOT{1:8}
- Specifies the return of the serial number for a module that is installed in an DCA-X. For a two-slot module installed in slots 1 and 2, specify
SLOT1. For a two-slot module installed in slots 3 and 4, specifySLOT3. For the 86108A four-slot module, specifySLOT1. Specifying an invalid slot for a given type of module results in the string "Not Present" being returned.