:SYSTem:HAL?
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:SYSTem:HAL?
Description
Queries the type of FlexDCA that is running. This indicates the state of FlexDCA's Hardware Abstaction Layer (HAL). The following strings can be returned by the query:
DCAN1000- FlexDCA running on an N1000A.
DSCP- N1010A FlexDCA running on a PC.
FEYE- FlexEye session instance in Eye/Mask mode's FlexEye Independent Eye Acquisition.
FEYE added in FlexDCA revision A.05.41 and above.
FRT- Flex Real Time session instance in FlexRT mode.
FRT added in FlexDCA revision A.06.70 and above.
SIM-
Deprecated (Firmware revision A.01.80 and below). FlexDCA is in data simulation control state.