:SYSTem:PERSona:MODel
Instrument:
                                                N1010A
                                                N1000A
                                                DCA-M
                                            Meas. mode:
                                                Scope
                                                Eye
                                                Jitter
                                                TDR
                                            Flex Apps:
                                                FlexDCA
                                                FlexRT
                                            Command Syntax
:SYSTem:PERSona:MODel "model number"
"model number" is a string.
Query Syntax
:SYSTem:PERSona:MODel?
Description
Specifies the model number of this product. The value is restricted to one of two strings: "N1000A" or "N1010A". If FlexDCA is runing on an N1000A, the default model number is "N1000A". If FlexDCA is runing on a PC, the default model number is "N1010A".
Example Command Sequence
:SYSTem:PERSona:MODel "N1000A"
Requires FlexDCA revision A.04.50 and above.