:SYSTem:PERSona:MODel:DEFault
Instrument:
                                                N1010A
                                                N1000A
                                                DCA-M
                                            Meas. mode:
                                                Scope
                                                Eye
                                                Jitter
                                                TDR
                                            Flex Apps:
                                                FlexDCA
                                                FlexRT
                                            Command Syntax
:SYSTem:PERSona:MODel:DEFault
Query Syntax
:SYSTem:PERSona:MODel:DEFault?
Description
Sets the model identification string to its default value. If FlexDCA is runing on an N1000A, the default model number is "N1000A". If FlexDCA is runing on a PC, the default model number is "N1010A".
Requires FlexDCA revision A.04.50 and above.