:SYSTem:MODel?
Query Syntax
:SYSTem:MODel? [{FRAMe | SLOT{1:8}}]
Description
Returns the model number of FlexDCA, a plug-in module, or a DCA-M instrument that is installed in the N1000A. An example of a returned string is N1092A or 86108B.
- FRAMe
- When FlexDCA is connected to an N1000A instrument, the returned string will be
N1000A. When FlexDCA is not connected to an instrument, the returned string will beN1010A.FRAMeis the default command argument if no argument is provided. - SLOT{1:8}
-
For the specified slot, returns the model number of the installed hardware module or assigned DCA-M instrument. If a simulated module is assigned to a slot, the string "N1010A" is returned and, in this case, you can use the
:EMODules:SLOT:SELection?query to determine the type of simulated module. If a model number is returned, the:EMODules:DCAM:DEVice?returns two double quotes ("") if it is a installed hardware module or an identification string if it is an assigned DCA-M instrument.The string "Not Present" is returned if a module is not installed in the slot. For a multi-slot module, specify the left most slot. For example, for a module installed in slots 3 and 4, specify
SLOT3.If you are using FlexDCA on a PC to control FlexDCA on the N1000A (Flex-on-Flex), extended and simulated modules are:
- Recognized if installed in the PC's FlexDCA.
- Not recognized if installed in the N1000A's FlexDCA.
For FlexDCA revisions below 1.08.00, the returned string for the FRAMe argument will be N1010A when FlexDCA is installed on the oscilloscope.