:SYSTem:UTCNow?
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:SYSTem:UTCNow?
Description
Queries the Coordinated Universal Time (UTC) which was formerly GMT. The time is returned as a string with in the form of <month>/<day>/<year> <hour>:<minutes>:<seconds>. For example,
"12/10/2015 15:47:17"
which represents the 10th day of December 2015, with a time of 15th hour, 47 minutes, and 17 seconds.
Use the :SYSTem:TIME? query to return the current local time. Use the :SYSTem:DATE? query to return the date.
Requires FlexDCA revision A.05.30 and above.