Files

Instrument
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT

With FlexDCA, you can save many different types of information as shown in the table in this topic. Click the links in the table to discover how to save or load specific types of data files. Files saved within FlexDCA are saved to a default subfolders that is located in the user data folder. When FlexDCA is installed and embedded on the N1000A , the default user data folder is on the "D" partition. N1010A FlexDCA uses the same D:\User Files folders to save user files. FlexDCA files can be identified by the letter "x" in the file name extension. FlexDCA does not support MATLAB measurements or scripts, so the MATLAB Measurements and MATLAB Scripts folders are not used.

Remember to always copy important settings and waveforms to an external memory device. If your original files are damaged or lost, you can restore the files from the backup.

Back up your user files to prevent accidental loss of important data.

N1000A. Because the FlexDCA application and operating system are located on the C: drive, it is best to keep all of your files on the D: drive and avoid making modifications to the files or folders on the C: drive.

Saving a file … Loading a file …
Save dialog …
Screen image file —
Instrument setup file Click File > Open Instrument Setup
Waveform file Waveform file into memory
Color-Grade/Gray Scale CG/GS file into memory
Jitter database Click File > Jitter Data Memory
Jitter Spectrum Analysis (JSA) file —
Dedicated dialogs …
Documentation wizard file —
— Eye mask test file
— De-embedding network setup files
(Loaded into waveform signal processing's InfiniiSim transform simulation operators)
Limit line test files Limit line test file into editor
Limit test summary files —
TDR/TDT calibration files TDR/TDT calibration files
TDR mode S-Parameter data files Touchstone files (Loaded info Waveform Signal Processing's s2p and s4p operators)
User measurement files —
SCPI recorder files —