:CHANnel:TBASe:GENeral:METHod
Command Syntax
:CHANnelN:TBASe:GENeral:METHod {AUTO | ABSolute}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:TBASe:GENeral:METHod?
Description
For the indicated channel, selects the method used to define the waveform top and base definitions. The command is equivalent to setting the signal's Top-Base Definition in the Thresholds > General tab of the Configure Measurements dialog box.
- AUTO
- Specifies that the top (100%) and base (0%) levels be automatically determined using a histogram of the signal's amplitude values. This is the default setting.
- ABSolute
- Allows you to enter absolute values for the top-base levels. When
ABSoluteis selected, use the:CHANnel:THReshold:GENeral:TOPand:CHANnel:THReshold:GENeral:BASEcommands to enter the signal's top and base levels.
Example Command Sequence
:CHANnel1_2:THReshold:GENeral:TRACking OFF :CHANnel1_2:TBASe:GENeral:METHod ABSolute :CHANnel1_2:THReshold:GENeral:BASE -125E-3 :CHANnel1_2:THReshold:GENeral:TOP 125E-3