:CHANnel:THReshold:GENeral:STZero
Command Syntax
:CHANnelN:THReshold:GENeral:STZero {{ON | 1} | {OFF | 0}}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:THReshold:GENeral:STZero?
Query Response
{1 | 0}
Description
When you select the ± Hysteresis threshold definition for the selected signal (see :CHANnel:THReshold:GENeral:METHod), you can turn ON the :CHANnel:THReshold:GENeral:STZero setting to move thresholds within ±10 mV to zero. This feature is useful for differential signals.