:CHANnel:THReshold:GENeral:LOWer

Command Syntax

:CHANnelN:THReshold:GENeral:LOWer  <amplitude>

<amplitude> is a double.

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:THReshold:GENeral:LOWer?

Description

Sets or queries the General threshold's lower threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :CHANnel:THReshold:GENeral:PLOWer command.

Use the :CHANnel:THReshold:GENeral:METHod command to set waveform threshold levels to standard percentages or custom definitions.

Use the :CHANnel:THReshold:GENeral:UPPer command to enter a upper threshold level. Use the :CHANnel:THReshold:GENeral:MIDDle command to enter a middle threshold level.

Example Command Sequence

:CHANnel1_2:THReshold:GENeral:TRACking OFF
:CHANnel1_2:THReshold:GENeral:METHod ABSolute
:CHANnel1_2:THReshold:GENeral:UPPer 125E-3
:CHANnel1_2:THReshold:GENeral:MIDDle 0E0
:CHANnel1_2:THReshold:GENeral:LOWer -125E-3