:CHANnel:THReshold:GENeral:TRACking

Command Syntax

:CHANnelN:THReshold:GENeral:TRACking  {{ON | 1} | {OFF | 0}}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:THReshold:GENeral:TRACking?

Query Response

{1 | 0}

Description

Specifies whether a signal tracks the global threshold definition or uses its own threshold definition.

The global threshold definition is set using the :MEASure:THReshold:GENeral commands (see Threshold Configuration Commands).

Example Command Sequence

:CHANnel2:THReshold:GENeral:TRACking OFF
:CHANnel2:THReshold:GENeral:METHod ABSolute
:CHANnel2:THReshold:GENeral:UPPer 125E-3
:CHANnel2:THReshold:GENeral:MIDDle 0E0
:CHANnel2:THReshold:GENeral:LOWer -125E-3