:CHANnel:THReshold:GENeral:HYSTeresis

Command Syntax

:CHANnelN:THReshold:GENeral:HYSTeresis  <plus_or_minus_value>

<plus_or_minus_value> is a double.

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:THReshold:GENeral:HYSTeresis?

Description

When the :CHANnel:THReshold:GENeral:METHod setting is HYSTeresis, this command sets the user-defined ±hysteresis value for the waveform source

Use the :CHANnel:THReshold:GENeral:MIDDle command to enter the center threshold level.

Example Command Sequence

:CHANnel1_2:THReshold:GENeral:TRACking OFF
:CHANnel1_2:THReshold:GENeral:METHod HYSTeresis
:CHANnel1_2:THReshold:GENeral:HYSTeresis 125E-3
:CHANnel1_2:THReshold:GENeral:MIDDle 0E0