:CHANnel:THReshold:RFALl:PLOWer

Command Syntax

:CHANnelN:THReshold:RFALl:PLOWer  <percent>

<percent> is a decimal number from -25.0 to +125.0.

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:THReshold:RFALl:PLOWer?

Description

When the threshold method is a custom PERCent between top and base (see :CHANnel:THReshold:RFALl:METHod), the :CHANnel:THReshold:RFALl:PLOWer command sets or queries the custom lower percent value.

Example Command Sequence

:CHANnel1_2:THReshold:RFALl:TRACking OFF
:CHANnel1_2:THReshold:RFALl:METHod PERCent
:CHANnel1_2:THReshold:RFALl:PUPPer 125E-3
:CHANnel1_2:THReshold:RFALl:PLOWer -125E-3