:CHANnel:THReshold:RFALl:TOP
Command Syntax
:CHANnelN:THReshold:RFALl:TOP <amplitude>
<amplitude> is a double.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:THReshold:RFALl:TOP?
Description
For the indicated channel, sets or queries the Rise/Fall threshold's custom top-level setting. The top and base levels are used to locate a waveform's lower and upper threshold levels for the rise time, fall time, and slew rate measurements. Specify the level in volts or Watts depending on the waveform type. Use :CHANnel:THReshold:RFALl:BASE to set or query a custom base level.
Before this user-defined top level can be applied to measurements, use the :CHANnel:TBASe:RFALl:METHod command to select user-defined top-base definitions.
The default setting is 240 mV. The maximum setting is 429 mv. The minimum setting can be -429 mV but is bounded by the base level (:CHANnel:THReshold:RFALl:BASE).
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.
Example Command Sequence
:CHANnel1_2:THReshold:RFALl:TRACking OFF :CHANnel1_2:TBASe:RFALl:METHod ABSolute :CHANnel1_2:THReshold:RFALl:BASE -125E-3 :CHANnel1_2:THReshold:RFALl:TOP 125E-3