:CHANnel:THReshold:GENeral:PAM:THResholds:EYE

Command Syntax

:CHANnelN:THReshold:GENeral:PAM:THResholds:EYE{0:2}  <amplitude>

Where <amplitude> is a double.

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:THReshold:GENeral:PAM:THResholds:EYE{0:2}?

Description

When specifying PAM general thresholds and you select the ± Hysteresis threshold definition for the selected signal (see :CHANnel:THReshold:GENeral:METHod), this command sets or queries the PAM eye threshold level. This value is used when making measurements.

Use the :CHANnel:THReshold:GENeral:HYSTeresis command to specify the amount of hysteresis.

Use the :CHANnel:THReshold:GENeral:PAM:ASTHresholds command to automatically set the PAM thresholds and hysteresis using a vertical histogram measurement.