:CHANnel:THReshold:RFALl:PAM:PAMLevel:LEVel
Command Syntax
:CHANnelN:THReshold:RFALl:PAM:PAMLevel:LEVel{0:3} <amplitude>
Where <amplitude> is a double.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:THReshold:RFALl:PAM:PAMLevel:LEVel{0:3}?
Description
When specifying PAM rise/fall levels and you have selected the Absolute level method for the selected signal (see :CHANnel:TBASe:RFALl:METHod), this command sets or queries the PAM level values.
Use the :CHANnel:THReshold:RFALl:PAM:ASLevels command to automatically set the PAM levels.