:CHANnel:THReshold:RFALl:LOWer
Command Syntax
:CHANnelN:THReshold:RFALl:LOWer <amplitude>
<amplitude> is a double.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:THReshold:RFALl:LOWer?
Description
Sets or queries the Rise/Fall threshold's lower threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :CHANnel:THReshold:RFALl:PLOWer command.
Use the :CHANnel:THReshold:RFALl:METHod command to set waveform threshold levels to standard percentages or custom definitions.
Use the :CHANnel:THReshold:RFALl:UPPer command to enter a upper threshold level.
Example Command Sequence
:CHANnel1_2:THReshold:RFALl:TRACking OFF :CHANnel1_2:THReshold:RFALl:METHod ABSolute :CHANnel1_2:THReshold:RFALl:UPPer 125E-3 :CHANnel1_2:THReshold:RFALl:LOWer -125E-3