:CHANnel:THReshold:GENeral:MIDDle
Command Syntax
:CHANnelN:THReshold:GENeral:MIDDle <amplitude>
Where <amplitude> is a double.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:THReshold:GENeral:MIDDle?
Description
Sets or queries the middle threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :CHANnel:THReshold:GENeral:PMIDdle command.
Use the :CHANnel:THReshold:GENeral:METHod command to set waveform threshold levels to standard percentages or custom definitions.
Use the :CHANnel:THReshold:GENeral:UPPer command to enter a upper threshold level. Use the :CHANnel:THReshold:GENeral:LOWer command to enter a lower threshold level.
Example Command Sequence
:CHANnel1_2:THReshold:GENeral:TRACking OFF :CHANnel1_2:THReshold:GENeral:METHod ABSolute :CHANnel1_2:THReshold:GENeral:UPPer 125E-3 :CHANnel1_2:THReshold:GENeral:MIDDle 0E0 :CHANnel1_2:THReshold:GENeral:LOWer -125E-3