:CHANnel:THReshold:GENeral:PAM:PAMLevel:LEVel

Command Syntax

:CHANnelN:THReshold:GENeral:PAM:PAMLevel:LEVel{0:3}  <amplitude>

Where <amplitude> is a double.

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:THReshold:GENeral:PAM:PAMLevel:LEVel{0:3}?

Description

When specifying PAM general levels and you have selected the Absolute level method for the selected signal (see :CHANnel:TBASe:GENeral:METHod), this command sets or queries the PAM level values.

Use the :CHANnel:THReshold:GENeral:PAM:ASLevels command to automatically set the PAM levels.