:CHANnel:THReshold:GENeral:PUPPer
Command Syntax
:CHANnelN:THReshold:GENeral:PUPPer <percent>
<percent> is a decimal number from -25.0 to +125.0.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:THReshold:GENeral:PUPPer?
Description
When the threshold method is a custom PERCent between top and base (see :CHANnel:THReshold:GENeral:METHod), the :CHANnel:THReshold:GENeral:PUPPer command sets or queries the custom upper percent value.
Example Command Sequence
:CHANnel1_2:THReshold:GENeral:TRACking OFF :CHANnel1_2:THReshold:GENeral:METHod PERCent :CHANnel1_2:THReshold:GENeral:PUPPer 125E-3 :CHANnel1_2:THReshold:GENeral:PMIDdle 0E0 :CHANnel1_2:THReshold:GENeral:PLOWer -125E-3