:CHANnel:THReshold:GENeral:AUTO

Command Syntax

:CHANnelN:THReshold:GENeral:AUTO

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

When you select the ± Hysteresis threshold definition for the selected signal (see :CHANnel:THReshold:GENeral:METHod), you can send :CHANnel:THReshold:GENeral:AUTO to automatically set the Center Threshold (:CHANnel:THReshold:GENeral:MIDDle) to be halfway between Vmin and Vmax and the Hysteresis value (:CHANnel:THReshold:GENeral:HYSTeresis) to be ±0.05(Vmax - Vmin).