:FUNCtion:PARameters:DFEQualizer:ATARgets
Command Syntax
:FUNCtionN:PARameters:DFEQualizer:ATARgets {ON | OFF | 1 | 0}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:DFEQualizer:ATARgets?
Query Response
{1 | 0}
Description
For the Decision Feedback Equalizer operator (DFE) (:FUNCtion:FOPerator), this command turns on and off automatically determined upper and lower targets in the DFE algorithm. By default, automatically determined upper and lower targets are on.
When off, use the :FUNCtion:PARameters:DFEQualizer:LTARget and :FUNCtion:PARameters:DFEQualizer:UTARget commands to specify the upper and lower target values.