:FUNCtion:PARameters:DFEQualizer:CLKDelay
Command Syntax
:FUNCtionN:PARameters:DFEQualizer:CLKDelay <delay_time>
<delay_time> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:DFEQualizer:CLKDelay?
Description
Sets the time delay for a Decision Feedback Equalizer operator (DFE) (:FUNCtion:FOPerator), which delays the decision point used by the slicer. The decision point is placed directly between the edges, so as to delay the edges.
Example Command Sequence
:FUNCtion1:FOPerator DFEQualizer :FUNCtion1:DISPlay ON :FUNCtion1:COLor TCOLor9 :FUNCtion1:PARameters:DFEQualizer:TAPS:AUTO ON :FUNCtion1:PARameters:DFEQualizer:TAPS:COUNt 5 :FUNCtion1:PARameters:DFEQualizer:TAPS:ULIMit 4.5E-1 :FUNCtion1:PARameters:DFEQualizer:TAPS:LLIMit -4.5E-1 :FUNCtion1:PARameters:DFEQualizer:CLKDelay 4.0E-12 :FUNCtion1:PARameters:DFEQualizer:BANDwidth:AUTO ON :FUNCtion1:PARameters:DFEQualizer:DTHReshold OFF