:FUNCtion:PARameters:DFEQualizer:TAPS:RECalculate

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:TAPS:RECalculate

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Initiates a re-calculation of the tap values for a Decision Feedback Equalizer operator (DFE) (:FUNCtion:FOPerator). Automatic tap configuration must be enabled (:FUNCtion:PARameters:DFEQualizer:TAPS:AUTO).

Example Command Sequence

:FUNCtion1:FOPerator DFEQualizer
:FUNCtion1:DISPlay ON
:FUNCtion1:COLor TCOLor9
:FUNCtion1:PARameters:DFEQualizer:TAPS:AUTO ON;*OPC?
:FUNCtion1:PARameters:DFEQualizer:TAPS:COUNt 5;*OPC?
:FUNCtion1:PARameters:DFEQualizer:TAPS:ULIMit 4.5E-1;*OPC?
:FUNCtion1:PARameters:DFEQualizer:TAPS:LLIMit -4.5E-1;*OPC?
:FUNCtion1:PARameters:DFEQualizer:CLKDelay 4.0E-12
:FUNCtion1:PARameters:DFEQualizer:BANDwidth:AUTO OFF
:FUNCtion1:PARameters:DFEQualizer:BANDwidth 1.0E+10
:FUNCtion1:PARameters:DFEQualizer:TAPS:RECalculate
:FUNCtion1:PARameters:DFEQualizer:DTHReshold OFF

Parent Command