:FUNCtion:PARameters:DFEQualizer:PROPtimize:TAPS

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:TAPS  "tap_value, tap_value, …"

The command argument is a string of comma separated list of real numbers (individual tap value).

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:TAPS?

Query Response

1.4582E-02,9.1E-05,1.85E-04

Description

When :FUNCtion:PARameters:DFEQualizer:PROPtimize is ON and :FUNCtion:PARameters:DFEQualizer:TAPS:AUTO is OFF, use this command to manually enter tap values for an optimized pulse response. For example, for three taps you might enter:

:FUNCtion1:PARameters:DFEQualizer:PROPtimize:TAPS "1.4582E-02,9.1E-05,1.85E-04"

Pulse response optimization (:FUNCtion:PARameters:DFEQualizer:PROPtimize) must be on to use this command.