:FUNCtion:PARameters:DFEQualizer:TLUNits

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:TLUNits {UNITless | VOLT}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DFEQualizer:TLUNits?

Query Response

{UNIT | VOLT}

Description

Chooses how you want to specify tap limit values with the :FUNCtion:PARameters:DFEQualizer:TAPS:ULIMit and :FUNCtion:PARameters:DFEQualizer:TAPS:LLIMit commands:

  • UNITless — You will enter unitless tap limit values.
  • VOLT — You will enter tap limit values in voltage.

Example Command Sequence

:FUNCtion1:FOPerator DFEQualizer
:FUNCtion1:DISPlay ON
:FUNCtion1:COLor TCOLor9
:FUNCtion1:PARameters:DFEQualizer:TAPS:AUTO ON
:FUNCtion1:PARameters:DFEQualizer:TAPS:COUNt 5
:FUNCtion1:PARameters:DFEQualizer:TLUNits UNITless
:FUNCtion1:PARameters:DFEQualizer:TAPS:ULIMit 5.00E-01,5.00E-01,5.00E-01,5.00E-01
:FUNCtion1:PARameters:DFEQualizer:TAPS:LLIMit -5.00E-01,-5.00E-01,-5.00E-01,-5.00E-01
:FUNCtion1:PARameters:DFEQualizer:CLKDelay 4.0E-12
:FUNCtion1:PARameters:DFEQualizer:BWMode TSBandwidth
:FUNCtion1:PARameters:DFEQualizer:DTHReshold OFF