:FUNCtion:PARameters:DFEQualizer:TAPS:AUTO
Command Syntax
:FUNCtionN:PARameters:DFEQualizer:TAPS:AUTO {ON | OFF | 1 | 0}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:DFEQualizer:TAPS:AUTO?
Query Response
{1 | 0}
Description
Turns on and off automatic configuration of taps for a Decision Feedback Equalizer operator (DFE) (:FUNCtion:FOPerator). By default, automatic configuration is on.
- OFF
- Disables automatic tap configuration to enable manual entry of tap values. Use the
:FUNCtion:PARameters:DFEQualizer:TAPScommand to enter the individual tap values. - ON
- Enables automatic tap configuration which sets the optimum tap values to open an eye diagram. This is the default setting. To enter the number of taps, use the
:FUNCtion:PARameters:DFEQualizer:TAPS:COUNtcommand. Use the:FUNCtion:PARameters:DFEQualizer:TAPS:RECalculatecommand to automatically recalculate the tap values.
Example Command Sequence
:FUNCtion1:FOPerator DFEQualizer :FUNCtion1:DISPlay ON :FUNCtion1:COLor TCOLor9 :FUNCtion1:PARameters:DFEQualizer:TAPS:AUTO ON;*OPC? :FUNCtion1:PARameters:DFEQualizer:TAPS:COUNt 5;*OPC? :FUNCtion1:PARameters:DFEQualizer:TAPS:ULIMit 4.5E-1;*OPC? :FUNCtion1:PARameters:DFEQualizer:TAPS:LLIMit -4.5E-1;*OPC? :FUNCtion1:PARameters:DFEQualizer:CLKDelay 4.0E-12 :FUNCtion1:PARameters:DFEQualizer:BANDwidth:AUTO OFF :FUNCtion1:PARameters:DFEQualizer:BANDwidth 1.0E+10 :FUNCtion1:PARameters:DFEQualizer:TAPS:RECalculate;*OPC? :FUNCtion1:PARameters:DFEQualizer:DTHReshold OFF