:FUNCtion:PARameters:DFEQualizer:PROPtimize:SAMPlitude

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:SAMPlitude

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:SAMPlitude?

Description

When :FUNCtion:PARameters:DFEQualizer:PROPtimize is ON and :FUNCtion:PARameters:DFEQualizer:TAPS:AUTO is OFF, use this command to enter Signal Amplitude for the optimized pulse response

Pulse response optimization (:FUNCtion:PARameters:DFEQualizer:PROPtimize) must be on to use this command.

Example

To enter 257.15 μW:

:FUNCtion:PARameters:DFEQualizer:PROPtimize:SAMPlitude "2.5715E-4"