:FUNCtion:PARameters:DFEQualizer:PROPtimize:MCURsor
Command Syntax
:FUNCtionN:PARameters:DFEQualizer:PROPtimize:MCURsor
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:DFEQualizer:PROPtimize:MCURsor?
Description
When :FUNCtion:PARameters:DFEQualizer:PROPtimize is ON and :FUNCtion:PARameters:DFEQualizer:TAPS:AUTO is OFF, use this command to enter Main Cursor Amplitude for the optimized pulse response.
Pulse response optimization (:FUNCtion:PARameters:DFEQualizer:PROPtimize) must be on to use this command.
Example
To enter 246.48 μW:
:FUNCtion:PARameters:DFEQualizer:PROPtimize:MCURsor "2.4648E-4"