:FUNCtion:PARameters:DFEQualizer:BANDwidth:AUTO
Command Syntax
:FUNCtionN:PARameters:DFEQualizer:BANDwidth:AUTO {ON | OFF | 1 | 0}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:DFEQualizer:BANDwidth:AUTO?
Query Response
{1 | 0}
Description
Turns on and off automatic bandwidth setting of the Gaussian filter for the Decision Feedback Equalizer operator (DFE) (:FUNCtion:FOPerator). To manually set the bandwidth, use the :FUNCtion:PARameters:DFEQualizer:BANDwidth command. By default, automatic configuration is on.
Example Command Sequence
:FUNCtion1:FOPerator DFEQualizer :FUNCtion1:DISPlay ON :FUNCtion1:COLor TCOLor9 :FUNCtion1:PARameters:DFEQualizer:TAPS:AUTO ON :FUNCtion1:PARameters:DFEQualizer:TAPS:COUNt 5 :FUNCtion1:PARameters:DFEQualizer:TAPS:ULIMit 4.5E-1 :FUNCtion1:PARameters:DFEQualizer:TAPS:LLIMit -4.5E-1 :FUNCtion1:PARameters:DFEQualizer:CLKDelay 4.0E-12 :FUNCtion1:PARameters:DFEQualizer:BANDwidth:AUTO ON :FUNCtion1:PARameters:DFEQualizer:DTHReshold OFF