:FUNCtion:PARameters:DFEQualizer:PROPtimize

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize {ON | OFF}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function (see :FUNCtion:FOPerator). The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize?

Query Response

{0 | 1}

Description

Turns the DFE equalizer's pulse optimization on or off. The following table shows the:

Required Conditions for :FUNCtion:PARameters:DFEQualizer:PROPtimize Child Commands
Child Command Auto Taps Pulse Optimization Description Associated Control Tab
Location in DFE Setup Dialog
OFF ON OFF ON
:FUNCtion:PARameters:DFEQualizer:PROPtimize:TAPS ■ ■ Enters the tap values. Taps
:FUNCtion:PARameters:DFEQualizer:PROPtimize:SAMPlitude ■ ■ Enter the signal amplitude. Taps
:FUNCtion:PARameters:DFEQualizer:PROPtimize:MCURsor ■ ■ Enters the main cursor amplitude. Taps
:FUNCtion:PARameters:DFEQualizer:PROPtimize:BMAX ■ ■ ■ Enters the tap limits (bmax(N)) values. Advanced
:FUNCtion:PARameters:DFEQualizer:PROPtimize:DELay ■ ■ ■ Enters the pulse delay (Dp) in UI. Pulse Response Tab
:FUNCtion:PARameters:DFEQualizer:PROPtimize:LENGth ■ ■ ■ Enters the pulse length (Np) in UI. Pulse Response Tab
:FUNCtion:PARameters:DFEQualizer:PROPtimize:SAVE ■ ■ Saves the pulse response to a file after optimization. Pulse Response Tab
:FUNCtion:PARameters:DFEQualizer:PROPtimize:SAVE:FILE ■ ■ Specifies the file to which to save the pulse response. Pulse Response Tab