:FUNCtion:PARameters:DFEQualizer:PROPtimize:LENGth

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:LENGth <UI>

Where <UI> is unit interval expressed as an integer.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:LENGth?

Description

When pulse response optimization (:FUNCtion:PARameters:DFEQualizer:PROPtimize) is on, sets the Pulse Length (Np) in UI. The default value is 200 UI. The minimum value is 8 UI and the maximum is 1000 UI.

Pulse response optimization (:FUNCtion:PARameters:DFEQualizer:PROPtimize) must be on to use this command.

Automatic taps (:FUNCtion:PARameters:DFEQualizer:TAPS:AUTO) can be on or off when using this command.