:FUNCtion:PARameters:DFEQualizer:SEED:VALue
Command Syntax
:FUNCtionN:PARameters:DFEQualizer:SEED:VALue <value>
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
<value> is a integer.
Query Syntax
:FUNCtionN:PARameters:DFEQualizer:SEED:VALue?
Description
When seeding of DFE taps is enabled (see :FUNCtion:PARameters:DFEQualizer:SEED), this command specifies the Seed Value that initial symbols are all seeded to so that the DFE can start working on the first UI.