:FUNCtion:PARameters:DFEQualizer:PROPtimize:BMAX

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:BMAX "limit, limit, …"

The command argument is a string of comma separated list of real numbers (limit values).

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:BMAX?

Description

Sets the maximum tap magnitudes (bmax(n)) for each tap, when tap magnitude limits are on (:FUNCtion:PARameters:DFEQualizer:PROPtimize:LTMagnitudes).

Sets the maximum tap values (bbmax(n)) for each tap, when tap magnitude limits are off (:FUNCtion:PARameters:DFEQualizer:PROPtimize:LTMagnitudes). To set the minimum tap values (bbmin(n)) for each tap, use the associated :FUNCtion:PARameters:DFEQualizer:PROPtimize:BMIN command.

Pulse response optimization (:FUNCtion:PARameters:DFEQualizer:PROPtimize) must be on to use this command.

Automatic taps (:FUNCtion:PARameters:DFEQualizer:TAPS:AUTO) can be on or off when using this command.