:FUNCtion:PARameters:DFEQualizer:UTARget

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:UTARget <voltage>

<voltage> is a Double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DFEQualizer:UTARget?

Description

When automatically determined upper and lower target values setting is off (see :FUNCtion:PARameters:DFEQualizer:ATARgets), use this command to specify the high logical value used in the DFE algorithm.

In DFE, when a bit is determined to be a logical high, its value will be equal to the UTARget.