:FUNCtion:PARameters:DFEQualizer:PRESets
Command Syntax
:FUNCtionN:PARameters:DFEQualizer:PRESets <string>
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Loads a previously saved a preset for a Decision Feedback Equalizer (DFE) operator. The preset configures the operator to your saved settings. To query which presets are available for loading, use the :FUNCtion:PARameters:DFEQualizer:PRESets:SELections? query.
Presets can only be saved from the operator's Setup dialog box. There is no programming command for this task.
Example Command
:FUNCtion:PARameters:DFEQualizer:PRESets "MyPreset" // Load a saved preset.